Reduce the magnification of a display
The
Zoom Out
option on the View
menu reduces the magnification of the display. This gives you an overview of the objects on the display.To reduce the magnification of a display
- From theViewmenu, selectZoom Out, or on the toolbar, select
.
TIP:
To return the display to its original size, from the
View
menu, select Cancel Zoom.
Provide Feedback