Magnify a display
The
Zoom In
option on the View
menu allows you to see the objects in an area of the graphic display in more detail, making it easier to draw.To magnify an area
- Select the object or objects to magnify.
- From theViewmenu, selectZoom In, or on the toolbar, select
.
Use the scroll bars to view the desired area of the graphic display.
TIP:
To return the display to its original size, from the
View
menu, select Cancel Zoom.
Provide Feedback