Set up the Graphics Display window
You can set up the Graphics Display window from the
View
menu.To set up the Graphics Display window
- From theViewmenu, toggle on or off the display of the Status bar, Explorer, and toolbars.
These settings apply to the
Graphics Display
window rather than the individual graphic displays. They stay as you set them from one editing session to the next.Provide Feedback