Set up a graphic display
You can set up a graphic display from the
Edit
menu, context menu, or View
menu.To set up a graphic display
- UseDisplay Settingson theEditmenu or context menu to define the size and background color for the graphic display. Some display settings also determine how the screen will look and behave at runtime.
- UseGrid Settingson theViewmenu to set up and activate a grid for the current graphic display.
- Use commands on theViewmenu such asZoom InorZoom Outto increase or reduce the magnification of the graphic display. Magnification is not retained between editing sessions.
Provide Feedback