Specify project settings (General tab)

On the
General
tab of the
Project settings
dialog box, specify the size of the project window and the application type.
To specify window appearance and application type
  • On the
    General
    tab of the
    Project settings
    dialog box, select the project window size from the list.
    TIP:
    If there are unsaved changes in the
    Alarm setup
    editor, or if the application exceeds the
    PanelView Plus 7 Standard
    or
    PanelView Plus 6 Compact
    application limits, do not convert the application to a
    PanelView Plus 7 Standard
    or
    PanelView Plus 6 Compact
    application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal