Specify project settings (Runtime tab)

On the
Runtime
tab of the
Project Settings
editor, specify the window elements that are shown at runtime, such as title bar and minimize button.
If you make changes to the title bar or border settings after you have created graphic displays, you will have the option of scaling the displays.
To specify window runtime settings
  1. On the
    Runtime
    tab of the
    Project settings
    dialog box, select the check boxes beside the window elements that you want the window to show at runtime.
  2. (Optional) Specify a project window position.
  3. (Optional) Select the
    Enable auto logout
    check box to enable auto logout.
  4. Specify how many minutes the terminal must be inactive before the automatic logout occurs. Enter a value (1-32767) or select a tag.
  5. (Optional) Specify a graphic display to open after the automatic logout.
    TIP:
    When the advanced automatic logout is enabled, the automatic logout settings on the
    Runtime
    tab of the
    Project Settings
    dialog box are disabled, but the controls are preserved.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal