About project settings

How do I open the Project Settings dialog box?
In the
System
folder in the
Explorer
window, double-click the
Project Settings
icon.
Project settings determine the general appearance of your runtime application, such as the size and position of the project window and whether a title bar appears in the project window.
TIP:
Project settings affect how your graphic displays look. Specify project settings before you create graphic displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal