Specify project settings (Inactivity tab)

On the
Inactivity
tab of the
Project Settings
editor, configure advanced automatic logout settings.
TIP:
When the advanced automatic logout is enabled, the automatic logout settings on the
Runtime
tab of the
Project Settings
dialog box are disabled, but the controls are preserved.
To set up advanced automatic logout settings
  1. On the
    Inactivity
    tab of the
    Project settings
    dialog box, select the
    Enable advanced inactivity actions
    check box.
  2. Select the
    Log out the current user after an inactivity period
    checkbox.
  3. Specify how many minutes the terminal must be inactive before the automatic logout occurs. Enter a value (1-32767) or select a tag.
  4. (Optional) Specify a graphic display to open after the automatic logout.
    Specify how many minutes the terminal must be inactive before the application navigates to the specified display. Enter a value (0-32767) or select a tag.
  5. (Optional) Specify a numeric tag to read the remaining inactivity time in seconds.
  6. (Optional) Specify a numeric tag to stop the inactivity actions from occurring indefinitely, and reset the inactivity timeout.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal