Options on the General tab
The following table shows the options on the
General
tab of the Project Settings
dialog box.Options | Descriptions |
|---|---|
Project window size | Select the size of the project window. Usually, the project is designed to completely fill the runtime terminal’s screen. Therefore, set the project window size to the resolution of the terminal in pixels. The project window size property is used for all Replace type graphic displays. If you change the window size after you have created graphic displays, you have the option of scaling the graphic displays.
|
Width | If you select the project window size Custom size , type the width of the window in pixels. |
Height | If you select the project window size Custom size , type the height of the window in pixels. |
Provide Feedback