Projects

A
FactoryTalk Design Workbench
project contains different components that you use to design, configure, program, visualize, and maintain your devices.
A
FactoryTalk Design Workbench
project contains the following key elements:
  • Controller programs with the main logic for the project, executing a set of instructions
  • Configuration settings for controllers, drives, I/Os, and project-specific settings
  • Variables that are both global and local
  • User-defined date types, including arrays, structures, and defined words
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal