Work in multiple sessions of FactoryTalk Design Workbench

Create or open separate projects at the same time using different sessions of
FactoryTalk Design Workbench
. With multiple sessions opened, you can:
IMPORTANT:
  • The same project cannot be opened in different sessions at the same time.
  • Simultaneous builds or POU verifications in multiple
    FactoryTalk Design Workbench
    sessions are not supported. Finish the build or verification in one session before starting in another session.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal