Close a project

Close a project after completing changes or close a project to open another project.
Prerequisites
  • Open a project using
    FactoryTalk Design Workbench
    .
To close a project
  1. From the menu bar, select
    File
    Close project
    .
  2. (optional) In
    Unsaved changes
    , select one of the following:
    • Save
      . Saves the changes and closes the project.
    • No
      . Discards the changes and closes the project.
    • Cancel
      . Reopens the project to make further changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal