Open an existing project

Use the
Welcome
page or the
File
menu to open a user project that was created in
FactoryTalk Design Workbench
.
You can open multiple sessions of
FactoryTalk Design Workbench
simultaneously, but each project can only be opened in one session.
Prerequisites
  • Close any open projects.
To open an existing project
  • Do one of the following:
    • On the
      Welcome
      page, from the
      Recent Projects
      list, select a project.
    • On the
      Welcome
      page, select
      Open project
      , select a project, and then select
      Open
      .
    • From the menu bar, select
      File
      Open project
      , select a project, and then select
      Open
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal