Project import and export

Export a
FactoryTalk Design Workbench
project that contains one or more devices. Once exported, the project can be imported to
FactoryTalk Design Workbench
when the controller is offline.
By default, the project is exported to the Downloads folder with the name
<project-name>.ftdwa
.
An exported project maintains the general structure of the project and might include the following project configuration options and program elements:
  • Configuration options
    • Controller configuration
    • Class1 device configuration
    • I/O module configurations
    • Interrupts
  • Program elements
    • Programs
    • Function blocks
    • Global variables
    • Local variables
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal