Save a copy of the current project

Use
Save as
to save a copy of the current project with a different project name in the FTDW folder within Documents.
To save a copy of the current project
  1. From the menu bar, select
    File
    Save as
    .
  2. In
    Save as
    , enter the project name, and then select
    Create
    .
    TIP:
    Naming conventions are as follows:
    • The project name can contain up to 40 characters.
    • The project name is restricted to alphanumeric characters and underscores.
    • The project name cannot end with an underscore or contain consecutive underscores.
    • The project name cannot be reserved words for Windows or Disk Operating System, such as "nul", "aux", "con", "com1", and "lpt1".
After saving a copy of the current project, the original project is closed, and the new project is opened.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal