Delete projects

Use
Project manager
to delete projects and all the associated settings, files, and folders.
Prerequisites
  • The projects to be deleted are closed.
To delete projects
  1. From the
    File
    menu, select
    Project manager
    .
  2. In
    Project manager
    , select one or more projects that you want to delete, and then select
    Delete
    .
  3. In
    Delete project
    , select
    Delete
    .
    You can also delete a project by deleting the
    <project-name>
    folder in the FTDW folder within Documents.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal