Import and export project elements

Import and export project elements to transfer the elements from one project to another. Depending on the element type, the file formats for import and export are different.
File format for import and export
Project Element
File Format
Micro800
controller programs
M8A
Micro800
controller user-defined function blocks
M8A
Micro800
controller user-defined functions
M8A
Micro800
controller global or local variables
CSV or XLSX
Micro800
controller user-defined data types
M8A
Micro800
controller data logs
M8A
Micro800
controller recipes
M8A
Micro800
controller configuration - Modbus mapping
CSV
Micro800
controller configuration -
MicroLogix™
mapping
CSV
Micro800
controller configuration - DNP3 mapping
CSV
Micro800
controller configuration - DNP3 data set descriptor
M8A
Micro800
controller configuration - DNP3 data set prototype
M8A
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal