Import controllers, programs, function blocks, variables, or user-defined data types

Depending on the element type, the file formats for importing and exporting are different.
  • The following elements are imported from an M8A file:
    • Programs, including local variables and interrupts
    • Function blocks, including local variables
    • Functions, including local variables
    • User-defined data types, including array data types, structure data types, and defined words
    • Data logs
    • Recipes
  • The following elements are imported from a CSV or XLSX file:
    • Modbus mappings
    • MicroLogix mappings
    • DNP3 mapping
    • Global and local variables
    Via CSV or XLSX files, you can manipulate the data and edit a large variable data set.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal