Save a project

Save your project to preserve the current device state and program configurations to the FTDW folder within Documents.
To save a project
  • Do one of the following:
    • From the menu bar, select
      File
      Save
      .
    • From the toolbar, select Save icon.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal