Build a project and view outputs

FactoryTalk Design Workbench
builds the entire project before you download the program to the
Micro800
controller. After the initial build,
FactoryTalk Design Workbench
decides whether to rebuild the entire project or only the components that have changed since the last build before downloading.
We recommend that you manually build the project before downloading to find and resolve any errors.
Prerequisites
  • Save the project.
  • No download operation is in process.
To build a project and view outputs
  1. Build the project by doing one of the following:
    • In
      Project Organizer
      , right-click the controller node, and then select
      Build
      .
    • In
      Project Organizer
      , select the controller node, and then from the menu bar, select
      Device
      Build
      .
    • On the controller memory configuration page, select
      Build
      .
    • In
      Project Organizer
      , right-click an individual Program Organization Unit, and then select
      Verify Program
      .
  2. In the
    Output
    pane, on the
    Log
    page, monitor the building progress and identify build errors. If the project has build errors:
    1. In the
      Output
      pane, on the
      Error list
      page, view and resolve any build errors.
    2. Clean the build errors by doing one of the following, and then build again:
      • In
        Project Organizer
        , right-click the controller node, and then select
        Clean
        .
      • From the menu bar, select
        Device
        Clean
        .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal