Manage computers
Use .
FactoryTalk Administration Console
to manage the computer accounts in a FactoryTalk
network directory. The FactoryTalk
local directory
does not make use of computer accounts because all activity on the directory is restricted
to the local computer. For more information about the naming conventions for computers, see
New computer in FactoryTalk Services Platform
Help
TIP:
Starting from version 6.31.00, FactoryTalk Services Platform provides Historical Usage to manage computers in the FactoryTalk system.
Tasks related to managing computers:
- View computers' historical usage of the FactoryTalk system
- Add group memberships
- Remove group memberships
- Change the name of a client computer
- Change the name of a server computer
- Set the override directory cache policies
- Override the enable syslog system policyIMPORTANT:Managing computers requires explicit permissions. To verify permissions, inFactoryTalk Administration ConsoleExplorer, expandSystem, then right-clickComputers and Groupsand selectSecurity.Confirm the permissions listed in the prerequisites for the task are present with the logged in user account.
Provide Feedback