Historical Usage
How do I open Historical Usage?
- Open FactoryTalk Administration Console.
- SelectTools > View Historical Usage.
FactoryTalk Services Platform provides Historical Usage to make FactoryTalk users, Windows-lined users, and computers in the FactoryTalk system easier to manage. To use Historical Usage, you must configure
Feature Security
of FactoryTalk Administration Console to grant the required permissions. Use Historical Usage to:Users tab | Computers tab |
---|---|
|
|
IMPORTANT:
- Historical Usage will not display information for Windows users that are members of Windows-linked groups that have been added to the FactoryTalk Directory.
- You can only use Historical Usage to delete a Windows-linked user from the FactoryTalk Directory. It is not available to disable and enable a Windows-linked user using Historical Usage.
- You must have theList ChildrenandReadpermission for theComputersandUsersfolder.
Provide Feedback