Meanings of the column headings on the Computers tab

The following table shows the meanings of the column headings on the
Computers
tab.
Headings
Descriptions
Computer name
Shows the computer name.
Status
Shows the computer statuses, including:
  • Connected
  • Disconnected
Last logon time
Shows the date and time that the computer was last used to log in to the FactoryTalk system.
Last logon user
Shows the last user account that was used to log in to the FactoryTalk system from the specific computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal