Change a computer name in the FactoryTalk network directory
Use
Computer Properties
to modify the name of a computer, its description, and the computer groups to which it belongs. If a computer participating in a FactoryTalk
network directory has an account in the Network Directory, and if the name of that computer changes, update the computer account in the Network Directory to match the new Windows
computer name for that computer. Computer and computer group accounts are not linked to Windows
computer accounts and do not automatically update.Prerequisites
Changing a computer name in the
FactoryTalk
network directory requires these permissions:- Common > List Children
- Common > Read
- Common > Write
- Membership in the Administrator group.
To change a computer name in the
FactoryTalk
network directory- Use a different computer than the one whose name was changed inWindowsto log on to theFactoryTalknetwork directory. This computer must have an account in theFactoryTalk DirectoryTIP:If no other computer has an account in theFactoryTalk Directory, run theon the computer whose name has changed to add an account for the local computer and skip the rest of these steps.FactoryTalk DirectoryConfiguration Wizard
- InFactoryTalk Administration ConsoleExplorer, expandSystem>Computers, right-click the computer account whose name you need to change, and then selectProperties.
- InComputer name, type the newWindowscomputer name for the computer, or selectBrowseto select the computer, and then selectOK.
Provide Feedback