Security Settings-Permissions
How do I open Security Settings?
- InFactoryTalk Administration ConsoleExplorer, right-click the resource and then selectSecurity.
Use the
Permissions
tab in the Security Settings
dialog box to specify permissions that indicate which users or groups can perform actions on a resource, optionally from a specific computer or group. Permissions determine:- who (what user or group of users)
- located where (on what computer or group of computers)
- can do what (perform what actions) with the resource
Right-click an item in the
Explorer
, and select Security
to set the security permissions for the resource.
IMPORTANT:
Right-clicking the
System
folder, Users and Computers
folder, Users
folder, or the Computers
folder, and specifying security permissions sets security on that actual folder-it does not limit users’ access to the system.To limit access to resources in the
FactoryTalk
system, right-click the resource, select Security
and specify security permissions for the user and computer accounts.Security for computers cannot be specified in a Local Directory.
Setting | Description |
---|---|
View permissions by | Select User to select a user, and specify what actions that user can perform.Select Action to select an action, and specify which users can perform the action. |
Actions list | Expand the category that contains the action to secure and select the action. |
Users list | Select a user or user-computer pair from this list. After selecting a user and action, specify permissions. Select Allow or Deny , or clear both. Clear both Allow and Deny to make the area inherit its security settings from a resource higher in the FactoryTalk Directory tree. If Do not inherit permissions is selected, access is denied. |
Allow and Deny check boxes | To allow a user to perform the action, select Allow .To deny a user access to the action, select Deny .To make the resource inherit its security settings for the action from a resource at a higher level in the FactoryTalk Network Directory or FactoryTalk Local Directory tree, clear Allow and Deny . |
Add | Select Add to select a user or group of users, and a computer or group of computers. |
Remove | Select Remove to remove the selected user-computer pair from the Users list. |
Do not inherit permissions | This setting does not appear when configuring security on the FactoryTalk Directory itself, or when configuring feature security for product policies.Select Do not inherit permissions to break the chain of inheritance for permissions assigned to this resource. Clear to make the resource inherit permissions from higher levels in the FactoryTalk network directory or FactoryTalk local directory tree.Permissions inherited from higher levels do not override permissions specified explicitly for the resource. Explicit permissions always override inherited permissions, so breaking the chain of inheritance may not be necessary. |
Provide Feedback