Select Computer

How do I open Select Computer?
  1. Navigate to either
    New Computer Group
    or
    Computer Group Properties.
  2. In the
    General
    tab, click
    Add
    .
Use
Select Computer
to choose one or more computer accounts to add to a computer group. The available computer accounts are listed.
Select
Create New
to create a new computer account if needed. The new computer account will be added to the available computer list and can be selected to add to the computer group, it is not automatically added to the group.
After selecting the computer accounts from the list, select
OK
to finish adding those computers to the group.
Once a computer belongs to a computer group, it inherits the group's security settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal