Add a computer group
Create a computer group to simplify administration of computer accounts, and to set security permissions for a group of computers. Example: Restricting access to resources according to physical location by defining groups for the location and setting policies that require connection to the network. Add computer accounts to a group at any time, the individual accounts in the group will inherit the security settings of the group once added.
IMPORTANT:
Do not allow use of
Windows
Remote Desktop where line-of–sight security is required, because the location of the computer from which the user is operating the system cannot be established reliably. This can have unexpected results. For example, if you have restricted write security for the remote user’s computer, the local user could be denied access unexpectedly because the remote computer’s session persists after the remote user has logged off.Required security permissions
Adding computer group accounts requires these permissions:
- Common > Create Children
- Common > List Children
- Common > Read
To add a computer group
- InFactoryTalk Administration ConsoleExplorer, expand theFactoryTalknetwork directory tree, and then expand theSystemfolder until theComputer Groupsfolder is visible.
- Right-clickComputer Groups, and then selectNew Computer Group.
- InNew Computer Group, inNametype a name for the group account.
- (optional) InDescription, type a description of the group account. Example:Southeast Region, Building 25, packaging system)
- SelectOK.
Provide Feedback