Develop a user-specific interface

Develop a user-specific interface

Provide personalized user experience and make certain interface areas accessible only for particular user groups.
Application example
The is only visible for logged-in administrators.
NOTE:
Download a sample project:
UserSpecificInterface.zip
Prerequisites
  • Configure users and groups in the following way:
    User name
    Password
    Groups
    Admin1
    admin
    Admins
    User1
    user
    Users
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal