Open the project in an external code editor

Open the project in an external code editor

You can open the entire project in an external code editor.
Prerequisites
Set the default external code editor. See Set the default code editor.
  • To open the project in an external code editor
  • From the main toolbar, select
    Open .NET Solution
    .
    The default external code editor opens.
    TIP: Rockwell Automation recommends using
    Visual Studio®
    2022 or
    Visual Studio Code
    as the default code editor. Some development assistance features may not be available when using a different code editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal