Edit a data logger

Edit a data logger

Edit an existing data logger.
  1. To edit a data logger
  2. From the toolbar, select
    Open dashboard page
    .
  3. In the editor, select
    Configure a data logger
    .
  4. Select the data logger to edit.
  5. If needed, edit the logger
    Name
    and properties.
  6. Select
    Next
    .
  7. If there is no database for the logger, create a database:
    TIP: You can also right-click an existing database and select
    Duplicate
    . Duplicating a database is useful if you want to create a database based on an existing database.
    1. Select
      New database
      and complete:
      • Name
        . A name for the database.
      • Type
        . Either
        Embedded
        or
        ODBC connection
        .
    2. Select
      Next
      .
    3. Set the database properties.
    4. Select
      Next
      .
  8. Select the database to store the logger data and select
    Next
    .
  9. Select the variables that you want to log and select
    Next
    .
    TIP: You can find variables by using the search field.
  10. Select
    Exit
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal