Create a key value converter

Create a key value converter

Create a converter that changes Boolean values into localized text.
  1. In
    Project view
    , right-click
    Converters
    and select
    New
    Key-value converter
    .
  2. Double-click the converter.
  3. In the editor, set the following values:
    Keys
    Boolean
    Values
    String
    True
    True
    False
    False
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal