Develop a persistent setting specific to a user

Develop a persistent setting specific to a user

Create a checkbox that shows or hides a clock label, which state is persistent based on the currently logged in user.
Application example
NOTE:
Download a sample project:
UserSpecificPersistentSetting.zip
Prerequisites
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal