Configure a dropdown button

Configure a dropdown button

Configure a
Dropdown button
object by linking it with a container object type.
  1. In
    Project view
    , create a container object type to display when you select the dropdown button.
    For more information, see Create a graphic object type.
    For example, create a panel type.
  2. In
    Project view
    , in
    UI
    , right-click a container and select
    New
    Containers
    Dropdown button
    .
  3. In
    Properties
    , create a dynamic link between the
    Panel
    property and the container object type.
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal