Add a panel loader and a NetLogic

Add a panel loader and a NetLogic

Create a panel loader and add the Change Page From Tag NetLogic.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Containers
    Panel loader
    .
  2. From the toolbar, select
    Template Libraries
    .
  3. In
    Libraries
    , search for
    Change Page From Tag
  4. Under
    Components
    , drag
    Change Page From Tag
    to
    MainWindow (type)
    .
  5. In
    Properties
    :
    1. Create a dynamic link between
      PanelLoader
      and
      ProjectName
      UI
      MainWindow (type)
      PanelLoader1
      .
    2. Create a dynamic link between
      PageChangeTag
      and
      ProjectName
      Model
      Variable1
      .
    3. Create a dynamic link between
      ScreensFolder
      and
      ProjectName
      UI
      Screens
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal