Configure a sparkline

Configure a sparkline

Configure the source of the data to display in the Sparkline object. Adjust the Sparkline object properties.
IMPORTANT: Do not use polylines as containers for sparklines.
  1. In
    Project view
    , right-click a node to contain the
    Sparkline
    object and select
    New
    Data controls
    Sparkline
    .
  2. In
    Properties
    , create a dynamic link between
    Pen value
    and a node or database from which you want to obtain the data.
    For more information about dynamic links, see Create dynamic links.
  3. (optional) Configure the sparkline properties:
    • Pen color
      . Sparkline pen color.
    • Pen thickness
      . Sparkline pen thickness.
    • Time window
      . Sparkline time range.
    • Refresh time
      . Sparkline refresh time.
    • Y-axis maximum
      . Maximum value of the Y-axis.
    • Y-axis minimum
      . Minimum value of the Y-axis.
    • Range high
      . High value of the range.
    • Range low
      . Low value of the range.
    • Range color
      . Range background color.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal