Develop a label that displays the current date and time

Develop a label that displays the current date and time

Create a label and a dynamic link to a variable exposed by ClockLogic or System to display current date and time at runtime.
Application example
Application that displays current date and time at runtime.
TIP:
You can download a sample project from:
DisplayCurrentDateTime.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal