Configure a REST API Client

Configure a REST API Client

Add a REST API Client NetLogic from Libraries to expose HTTP methods.
  1. From the toolbar, select
    Template Libraries
    .
  2. In
    Libraries
    , search for
    REST API Client
    .
  3. Under
    Components
    , drag
    REST API Client
    onto
    NetLogic
    in
    Project view
    .
    In
    Project view
    ,
    RESTApiClient
    appears in the
    NetLogic
    folder.
  4. Close
    Libraries
    .
  5. (optional) In
    Properties
    edit:
    • Timeout
      . Time after the request is canceled if no response is received. Defaults to ten seconds.
    • UserAgent
      . String that represents the application from which the request originates. Defaults to FTOptix.
Use the exposed GET, POST, and PUT methods in your application logic. See HTTP methods.
TIP: For example, you can trigger the methods with a MouseClick event of a Button object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal