FactoryTalk View SE Client object model

The
FactoryTalk View SE
Client object model provides a way to manipulate the graphic objects on a display at runtime and to have programmatic access to tag properties.
Using the
Microsoft
Visual Basic for Applications Integrated Design Environment (VBA IDE), you can write display code that uses the Graphic objects in the
FactoryTalk View SE
Client object model to interact with the objects on displays at runtime, as well as load, hide, and unload displays. In addition, you can create tag groups, read and write tag values, receive notification when a tag value or quality changes, and access extended properties for HMI tags.
You cannot create new graphic or tag objects, or edit existing objects, with the
FactoryTalk View SE
Client object model. Any changes you make to a display and its objects at runtime are not saved. For example, if you change the position of an object on a display, the next time the display is loaded, the object will be in its original position. This does not apply to ActiveX controls which might save property changes after a test run has changed them.
Remarks
  • The
    FactoryTalk View SE
    Client object model provides an automation interface into the Graphics and Tag subsystems and is intended to be used primarily with VBA code and ActiveX controls.
  • Display code is associated with a particular display and is stored with it.
IMPORTANT:
Prior to running any VBA code, please verify and ensure your VBA codes are safe and trusted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal