MQTT objects
MQTT objects that are part of the FactoryTalk View SE Client object model provide programmatic capabilities to configure FactoryTalk View SE as an MQTT subscriber or publisher and the properties at runtime.
The supported MQTT versions are 5.0 and 3.1, and the supported protocols are TCP and WebSocket without TLS.
Provide Feedback