TrendPro object

The TrendPro object represents a TrendPro graphic object on a display. It is not a creatable object. It is accessed by the name assigned to it via the Panel.
The TrendPro object's properties and methods listed are available in VBA.
Properties
Methods
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal