DataGrid object
Represents a data grid object on a display. It is accessed by the name assigned to it via the Panel.
The DataGrid object's properties and methods listed are available in VBA.
Properties
Methods
Provide Feedback