SignatureButton object
The SignatureButton object represents the Signature Button ActiveX object. It is not a creatable object, that is you cannot use the New keyword to create an instance of the object.
The object is for use in a FactoryTalk View SE graphic display and is not designed to function on a VBA form.
Properties
Methods
Events
Constants
Provide Feedback