XY Plot object

The XY Plot object represents an XY Plot graphic object on a display. It is not a creatable object. It is accessed by the name assigned to it via the Panel.
The XY Plot object's properties and methods listed are available in VBA.
Properties
Methods
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal