Folder object
Represents a folder within the hierarchy of the HMI tag database. Use the object to access any subfolders that the folder may contain.
It is not a creatable object.
To obtain a reference to a Folder object, use the CreateFolder
, DuplicateFolder
, and GetFolder
methods of the TagDB object, or the Item
and Add
methods of the Folders collection.Properties
Provide Feedback