TagDB object
Represents an HMI tag database. Use the object to manage tags and folders in the tag database.
TIP:
Modify the tag database from one instance at one time, such as
FactoryTalk View SE
Client, FactoryTalk View Studio
, Tags editor, or the Tag Import and Export Wizard. Otherwise, errors may occur and you may not be able to modify.It is not a creatable object.
To obtain a reference to a TagDB object, use one of the following:- The global variableTagDBthat is only exposed in VBA and accessible in the current HMI tag database.
- TheTagDBproperty of the Display object or the Tag object.
Properties
Methods
Provide Feedback