Application object
The Application object represents an instance of the FactoryTalk View SE Client. There is one application object per FactoryTalk View SE Client instance.
The Application object is not a creatable object. The Application object is accessible through the Application property of the objects in the Graphic and Tag object models.
Properties
Methods
Events
Provide Feedback