Login event
Occurs when a user logs on.
Syntax
Application
_Login
(ByVal
UserName
As String
)where
Application
– is the name of a FactoryTalk View SE Client Application object variable that was dimensioned using the WithEvents keyword.UserName
– is the name of the user that logged on.Remarks
- When testing the animation of displays in the Graphics editor, this event does not fire because users cannot log on while testing a display.
- A Login event is only received by VBA if a display is open. This means that the event is not fired when a user is logged on during a FactoryTalk View SE Client startup because Login happens before a display is opened.
- A Login event will fire when the user logs on using the Login command, because the current display remains open.
Provide Feedback