Login method

Logs on the specified user.
Syntax
Application
.
Login
UserName
,
Password
where
Application
– is the name of a
FactoryTalk View SE
Client Application object or an expression that evaluates to a
FactoryTalk View SE
Client Application object.
UserName
– is the name of the user that is logging on.
Password
– is the password of the user that is logging on
Remarks
  • If the logon fails, an error will be raised with Err.Number equal to gfxErrorLoginFailed.
  • When testing the animation in displays in the Graphic Display editor, calls to this method raise an error with Err.Number equal to gfxErrorTestAnimation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal