User-defined functions

Use the
User-Defined Functions
node in Project Organizer to create logic programs for an
Micro820
L20E,
Micro850
L50E, or
Micro870
L70E controller project in the following programming languages:
  • Function block diagram (FBD)
  • Ladder diagram (LD)
  • Structured text (ST)
User-defined functions (UDFs) define a simple calculation that requires only one output. Once created, it can be reused like other function blocks in
FactoryTalk Design Workbench
.
TIP: The UDF input parameters support the array and structured data types. The UDF output parameter only supports simple data types.
Use the
User-Defined Functions
node to:
Use the
<UDF-name>
node under
User-Defined Functions
to:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal