Add Program Organization Unit descriptions

Use the
Description
box in the
Properties
pane to document individual Program Organization Units (POUs). For example, you can document the implementation details of a POU.
Descriptions are automatically saved and stored in rich text format (*.rtf).
To add POU descriptions
  1. In
    Project Organizer
    , select the POU.
  2. In the
    Properties
    pane, in the
    Description
    box, enter the description.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal